cancel
Showing results for 
Search instead for 
Did you mean: 

TTCAN in STM32F767

DVicc.1
Associate II

Hello I have read on the reference manual that the CAN controller can be set to work as TTCAN by setting the TTCM bit. But comparing with the STM32H7 it seems that only the latter family has the TTCAN functionality.

Someone has experience with that ?

Regards

Dav

1 REPLY 1
Uwe Bonnes
Principal III

All non-FD CAN hardware has as an errata that TTCAN is not working. "BxCAN time triggered mode not supported"