Transfer from STM32f411RE to STM32F411ce
Hi there,
Recently if done a project regarding custom hid on a STM32F411RE Nucleo prototype board, this was successful. I have created my own pcb design but unfortunatly due the lack of availability of the STM32F411RE i was forced to go with the STM32F411CE QFN48. Adapted my board design and after populating my newly received boards i run into a snag. I adapted my original code to the 411CE alas its not popping up in my windows device list as a custom HID device. But it does show in DFU mode , i can upload my code through ST LINK. Debugger in CUBEIDE works fine. Just to keep it simple i made a bare project which only use the custom HID options out of CUBE IDE. Does behave exactly as described, but not showing up as Custom HID Device.
Might be a bit short sighted but i think it is not my PCB design,cause of the above behavior.
Maybe someone in here has some experience with the F411CE and can put me on the right track.
Thanks in advance.