2009-12-22 2:26 AM
Tool flasher Cortex M3
2011-05-17 4:33 AM
Hello,
I want to find a tool that can programme the flash of my STM32F101R6. When i make some recherche on the site of SEGGER : Jflash software=400€+ Flash ARM 600 ( that can programme in stand-alone). It's so expensive to us and we cant invest an amount like this in the beginning. Do you all have some goods ideas ? It should be the best if we can find out a tool who can programme without pc==> We have to use pc to programme it in the first time only and then the tool can work independent. Thanks all,2011-05-17 4:33 AM
Hi
I don’t have in mind some commercialized tools. But I guess this could be feasible using another STM32 acting as a programmer (master).Through a simple program inspired from the IAP programming application note you can program STM32 targets (slaves) through USART by the STM32 (master), so you can baypass the PC. Cheers.2011-05-17 4:33 AM
STLink should be very cheap. Or Wiggler, or Olimex tool?
2011-05-17 4:33 AM
If you don't want debug capability you could use the STM32F internal bootloader to load your code serially.
Seehttp://www.st.com/mcu/forums-cat-9233-23.html
for a tool/software. Here's thehttp://www.er-tronik.de/shop2/product_info.php?cPath=34&products_id=113
to the programmer. [ This message was edited by: swhite on 09-12-2009 20:24 ]2011-05-17 4:33 AM
Hi tran.thequyen,
there is a Free stand-alone Cortex M3 Flash Programming softeware,http://www.coocox.org/CoFlash_Programmer.htm
, Using an openhttp://www.coocox.org/Colink.htm
,based on the FT2232. It has an intuitive user interface with a traditional Windows graphical user interface (GUI), and a command line mode as well. Open JTAG hardware debugging probe,CooCox Colink:http://www.coocox.org/Colink.htm
Free Cortex M3 FlashProgrammer:,Cooperate on Cortex,providing free and open ARM development tools. [ This message was edited by: ahnniu on 10-12-2009 01:56 ]2011-05-17 4:33 AM
Thanks all
Your infos is very useful==> I'm studying about your solutions. Quyen2011-05-17 4:33 AM
Dear Quyen:
I had develope a stand-alone programmer:EP868,can use for program STM32 without PC. it support JTAG/SWD,and Uart ISP also. Further more, it support stand-alone program for STM8S also. with www.mcuisp.com, you can find more info. James Peng www.mcuisp.com