cancel
Showing results for 
Search instead for 
Did you mean: 

To get data from Invensense MPU9250 with I2C

kano
Associate
Posted on May 26, 2015 at 13:25

I'm trying to get data from Invensense MPU9250 with I2C on SC1 of stm32w108.

These are connected each other with 10k ohm register.

But it doesn't get data.

I coded as below.

Please tell me how to fix.

void SCinit(){

        GPIO_InitTypeDef GPIO_InitStruct;

        I2C_InitTypeDef I2C_InitStruct;

        

        GPIO_InitStruct.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2;

        GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_OD;

        

        I2C_InitStruct.I2C_ClockRate = 400000;

        

        GPIO_Init(GPIOB, &GPIO_InitStruct);

        I2C_Init(SC1_I2C, &I2C_InitStruct);

        

        I2C_Cmd(SC1_I2C, ENABLE);

}

void MPU9250_initialize(){

MPU9250_setClockSource(MPU9250_CLOCK_PLL_XGYRO);

MPU9250_setFullScaleGyroRange(MPU9250_GYRO_FS_250);

MPU9250_setFullScaleAccelRange(MPU9250_ACCEL_FS_2);

MPU9250_setSleepModeStatus(0);

}

void MPU9250_setClockSource(uint8_t source){

MPU9250_writeBits(MPU9250_RA_PWR_MGMT_1, MPU9250_PWR1_BIT_CLOCK_SELECT, MPU9250_PWR1_BIT_CLKSEL_LENGTH, source);

}

void MPU9250_setFullScaleGyroRange(uint8_t range){

MPU9250_writeBits(MPU9250_RA_GYRO_CONFIG, MPU9250_RANGE_CONFIG_START, MPU9250_RANGE_CONFIG_LENGTH, range);

}

void MPU9250_setFullScaleAccelRange(uint8_t range){

MPU9250_writeBits(MPU9250_RA_ACCEL_CONFIG, MPU9250_RANGE_CONFIG_START, MPU9250_RANGE_CONFIG_LENGTH, range);

}

void MPU9250_setSleepModeStatus(uint8_t status){

MPU9250_writeBit(MPU9250_RA_PWR_MGMT_1, MPU9250_PWR1_BIT_SLEEP, status);

}

void MPU9250_writeBits(uint8_t regAddr, uint8_t bitStart, uint8_t bitLength, uint8_t data){

uint8_t buff;

uint8_t mask;

MPU9250_i2C_BufferRead(&buff, regAddr, 1);

mask = 1 << bitStart;

mask--;

mask <<= bitLength;

data <<= bitStart;

data &= mask;

buff &= ~mask;

buff |= data;

MPU9250_i2C_ByteWrite(buff, regAddr);

}

void MPU9250_writeBit(uint8_t regAddr, uint8_t bitNum, uint8_t value){

uint8_t buff;

uint8_t mask;

MPU9250_i2C_BufferRead(&buff, regAddr, 1);

mask = 1 << bitNum;

buff = (value != 0) ? (buff | mask) : (buff & ~mask);

MPU9250_i2C_ByteWrite(buff, regAddr);

}

void MPU9250_getRawGyro(uint8_t* data){

MPU9250_i2C_BufferRead(data, MPU9250_RA_GYRO_XOUT_H, 6);

        //MPU9250_i2C_BufferRead(data, MPU9250_RA_PWR_MGMT_1, 6);

}

void MPU9250_getRawAccel(uint8_t* data){

MPU9250_i2C_BufferRead(data, MPU9250_RA_ACCEL_XOUT_H, 6);

}

void MPU9250_getRaw6axis(uint8_t* data){

MPU9250_getRawAccel(data);

MPU9250_getRawGyro(data + 6);

}

void MPU9250_i2C_BufferRead(uint8_t* buff, uint8_t regAddr, uint8_t num){

I2C_GenerateSTART(SC1_I2C);

        

        while (!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_CMDFIN));

I2C_Send7bitAddress(SC1_I2C, MPU9250_DEFAULT_SLAVE_ADDRESS, I2C_Direction_Transmitter);

while (!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_BTF));

I2C_SendData(SC1_I2C, regAddr);

while (!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_BTF));

                

I2C_GenerateSTART(SC1_I2C);

        while (!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_CMDFIN));

        

I2C_Send7bitAddress(SC1_I2C, MPU9250_DEFAULT_SLAVE_ADDRESS, I2C_Direction_Receiver);

while (!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_BTF));

        

        uint8_t count;

        

        for(count = 0; count < num - 1; count++){

          buff[count] = I2C_ReceiveData(SC1_I2C);

                

                while(!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_BRF));

                

                I2C_AcknowledgeConfig(SC1_I2C, ENABLE);

        }

        

        buff[num - 1] = I2C_ReceiveData(SC1_I2C);

        

        while(!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_BRF));

        

        I2C_AcknowledgeConfig(SC1_I2C, DISABLE);

        I2C_GenerateSTOP(SC1_I2C);

        

        I2C_AcknowledgeConfig(SC1_I2C, ENABLE);

}

void MPU9250_i2C_ByteWrite(uint8_t data, uint8_t regAddr){

I2C_GenerateSTART(SC1_I2C);

        

        while (!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_CMDFIN));

I2C_Send7bitAddress(SC1_I2C, MPU9250_DEFAULT_SLAVE_ADDRESS, I2C_Direction_Transmitter);

while (!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_BTF));

I2C_SendData(SC1_I2C, regAddr);

while (!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_BTF));

I2C_SendData(SC1_I2C, data);

while (!I2C_GetFlagStatus(SC1_I2C, I2C_FLAG_BTF));

I2C_GenerateSTOP(SC1_I2C);

}

main() of my source calls MPU9250_getRaw6axis() ciclicity.

And I2C_ReceiveData() always returns 0 any register i choose.

I apologize that I am biginner of micro controller and not good for english.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0