2012-07-07 5:03 PM
Hello, I bought a STM32-Discovery, but when I turn on, the power led blink, and then the LED goes off. The PC dont detect a new hardware..
I measure the voltage in the TP1 is 0,85V. I think the board has a short but yet I dont know locate. I think if I remove the D1 BAT60JFILM, I measure 5 VCC from usb.Somebody already had a problem equal?Regards