cancel
Showing results for 
Search instead for 
Did you mean: 

Timing to be reflected __disable_irq() and __enable_irq()

Fkasa.1
Associate II

We make below code.

The variable a is written from both main function and interrupt function.

When accessing variable a with the main function to realize exclusive control, interrupt disable and enable (__disable_irq(), __enable_irq()) are used.

How long does it take from the execution of the interrupt disable function to the reflection on the CPU at this time?

Or is there a mechanism to access the variable a after the interrupt disable is reflected in the structure of the CPU?

If there is a manual regarding the behavior after executing the interrupt prohibition function, please let me know.​

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Piranha
Chief II

> We can rest assured that there is somewhere in the text that shows that the above is guaranteed.

https://developer.arm.com/documentation/dai0321/latest

Section: "4.8 Disabling interrupts using CPS and MSR instructions". Also I recommend reading at least sections 4.5-4.9, especially the 4.9.

View solution in original post

8 REPLIES 8
TDK
Super User

What chip family? You can find cycles per instruction on the M0 and M4 cores, but the M7 core is not as simple to calculate. Even on the M0/M4 cores it is not always straightforward.

https://developer.arm.com/documentation/ddi0439/b/CHDDIGAC

Keep in mind the compiler is free to rearrange/optimize as it sees fit. Use volatile if you don't want a variable optimized out.

If you feel a post has answered your question, please click "Accept as Solution".
Fkasa.1
Associate II

@TDK​ 

Thank you for answering.

Currently We use M4 cores.

Even if interrupt disable is set in the register using __disable_irq(), We are concerned that variables will be accessed from the main function and interrupt function at the same time during the delay until the CPU actually disables interrupts.

You think there is a delay between __disable_irq and when interrupts get disabled? Why?
Gating access to a variable within those calls is sufficient to ensure no interrupts will be called or access it at the same time.
If you feel a post has answered your question, please click "Accept as Solution".

I think it takes a few CLKs to write the disable_irq register and it works.

If main function are interrupted between a few CLKs, program cause unexpected behavior.

>>Gating access to a variable within those calls is sufficient to ensure no >>interrupts will be called or access it at the same time.

We can rest assured that there is somewhere in the text that shows that the above is guaranteed.

Nikita91
Lead II

If your application is as simple as your example code, you can't have the behavior you describe.

Are you sure you don't use a disable/enable pair in a function called from inside a protected code?

Using __disable_irq() / __enable_irq() is dangerous.

You must save the PRIMASK before you disable, and restore PRIMASK to enable again.

Piranha
Chief II

> We can rest assured that there is somewhere in the text that shows that the above is guaranteed.

https://developer.arm.com/documentation/dai0321/latest

Section: "4.8 Disabling interrupts using CPS and MSR instructions". Also I recommend reading at least sections 4.5-4.9, especially the 4.9.

Thank you for answering.

We read this section, and This is what we were looking for.

We will use __disable_irq() and __enable_irq() with confidence from now on

That's right.

We need to check the PriMask in the actual code.