2009-05-02 3:28 AM
Timers in quadrature decoder mode
2011-05-17 4:10 AM
Hmm, after reading the data sheet, it seems that there's no pin for TIM2_CH1..
Is there a way to use CH3 / CH4 instead?!2011-05-17 4:10 AM
Hi!
I want to use an STM32F103ZE to control a 4 axis CNC machine (with DC servos and quadrature encoders). As I understand, I can use TIM2..5 to simultaneously capture the 4 encoder positions, but I wonder which pins to use. Would this be ok? : TIM2_CH1 Enc. 1 Phase A TIM2_CH2 Enc. 1 Phase B TIM3_CH1 Enc. 2 Phase A TIM3_CH2 Enc. 2 Phase B TIM4_CH1 Enc. 3 Phase A TIM4_CH2 Enc. 3 Phase B TIM5_CH1 Enc. 4 Phase A TIM5_CH2 Enc. 4 Phase B The Reference Manual is a little bit unclear here. Can the other timer channels 3/4 also be used for quadrature capture?! Or do I have to use TIMx_CH1/2? What do the signals TI3FP3, TI3FP4, TI4FP3 and TI4FP4 on page 270 do?! I can't find any other reference to them in the manual.. Also, the firmware library seems to lack an example program for quadrature capture. Greetings from Germany, Thomas Kindler