cancel
Showing results for 
Search instead for 
Did you mean: 

Timers & alternate functions

Brother Theo
Associate II
Posted on January 07, 2016 at 22:20

Hi,

Noob here, trying to get life out of some hardware. I got basic I/O working (blink an LED) but now I am trying to get timers and alternate functions to work, with no luck. I am testing on a Nucleo-F410RE just to get my feet wet. My Code:

#include ''stm32f4xx.h''
#include ''stm32f4xx_rcc.h''
#include ''stm32f4xx_gpio.h''
#include ''stm32f4xx_tim.h''
void TM_LEDS_Init(void) {
GPIO_InitTypeDef GPIO_InitStruct;
/* Clock for GPIOD */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
/* Alternating functions for pins */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_TIM4);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_TIM4);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_TIM4);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_TIM4);
/* Set pins */
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void TM_TIMER_Init(void) {
TIM_TimeBaseInitTypeDef TIM_BaseStruct;
/* Enable clock for TIM4 */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);
TIM_BaseStruct.TIM_Prescaler = 0;
/* Count up */
TIM_BaseStruct.TIM_CounterMode = TIM_CounterMode_Up;
TIM_BaseStruct.TIM_Period = 8399; /* 10kHz PWM */
TIM_BaseStruct.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_BaseStruct.TIM_RepetitionCounter = 0;
/* Initialize TIM4 */
TIM_TimeBaseInit(TIM4, &TIM_BaseStruct);
/* Start count on TIM4 */
TIM_Cmd(TIM4, ENABLE);
}
void TM_PWM_Init(void) {
TIM_OCInitTypeDef TIM_OCStruct;
TIM_OCStruct.TIM_OCMode = TIM_OCMode_PWM2;
TIM_OCStruct.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCStruct.TIM_OCPolarity = TIM_OCPolarity_Low;
TIM_OCStruct.TIM_Pulse = 2099; /* 25% duty cycle */
TIM_OC1Init(TIM4, &TIM_OCStruct);
TIM_OC1PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_OCStruct.TIM_Pulse = 4199; /* 50% duty cycle */
TIM_OC2Init(TIM4, &TIM_OCStruct);
TIM_OC2PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_OCStruct.TIM_Pulse = 6299; /* 75% duty cycle */
TIM_OC3Init(TIM4, &TIM_OCStruct);
TIM_OC3PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_OCStruct.TIM_Pulse = 8399; /* 100% duty cycle */
TIM_OC4Init(TIM4, &TIM_OCStruct);
TIM_OC4PreloadConfig(TIM4, TIM_OCPreload_Enable);
}
int main(void) {
/* Initialize system */
SystemInit();
/* Init leds */
TM_LEDS_Init();
/* Init timer */
TM_TIMER_Init();
/* Init PWM */
TM_PWM_Init();
while (1) {
}
}

Looking at the debugger I can see the timer value changing, but there no output. I can't verify id the timer output is actually changing, nor can I verify if I have the alternate function set up right. Help? --TimR
1 REPLY 1
Posted on January 07, 2016 at 22:35

F410RE? You mean the

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00102166.pdf

 or the

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00115249.pdf

?

Check the Data Sheet for the part to ensure that TIM4 comes out of the pins you've picked. I'm not seeing that connectivity.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..