2014-02-05 04:41 AM
Hi,
Kit using : STM32Discovery Board(STM32F100 controller)I have implemented the input capture mechanism for Timer15 channel 1. In which I set triggering for both falling and rising edge.Now I am trying to port the application to Timer2 channel 2. But the problem what I facing is, in Timer2 I can't find any option to trigger both edge. Only one edge triggering is possible. So is there any mechanism to enable both edge triggering for Timer2.Please help me to come out of the situation.....ThanksSooraj Mannangal