cancel
Showing results for 
Search instead for 
Did you mean: 

Timer input capture interrupt fires over and over - Not a late flag reset issue (probably)

Tobe
Senior III

My input capture interrupt is fired over and over again. But when i put a breakpoint in the interrupt, and resume from it, it does not happen anymore.

Timer setup:

 

 

	// TIM 3 Inputs (Pedal rot - PB5 / Torc PWM - PB1)
	my_GPIO_InitStruct.Pin = GPIO_PIN_5 | GPIO_PIN_1;
	my_GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	my_GPIO_InitStruct.Pull = GPIO_PULLUP;
	HAL_GPIO_Init(GPIOB, &my_GPIO_InitStruct);
	GPIOB->AFR[0] |= (	GPIO_AFRL_AFSEL1_1 |  	// AF2 (all)
						GPIO_AFRL_AFSEL5_1);
	__disable_irq();
	__HAL_RCC_TIM3_CLK_ENABLE();

	SET_BIT(  TIM3->CCMR1,  TIM_CCMR1_CC2S_0);
	SET_BIT(  TIM3->CCMR2, 	TIM_CCMR2_CC4S_0);	// channel is configured as input, tim_ic1 is mapped on tim_ti1, etc...
	// TODO: filter??
	SET_BIT(  TIM3->CCER,   TIM_CCER_CC2E |
							TIM_CCER_CC2NP |
							TIM_CCER_CC2P |
							TIM_CCER_CC4E |
							TIM_CCER_CC4NP |
							TIM_CCER_CC4P);		//  capture enable and Rising and falling edge

	// TISEL default input channels

	SET_BIT(  TIM3->DIER,   TIM_DIER_CC2IE | TIM_DIER_CC4IE); 	// enable interrupt on signal
	SET_BIT(  TIM3->CR1,    TIM_CR1_CEN); 		// enable counter timer 3

	NVIC_EnableIRQ(TIM3_IRQn);				// enable global interrupt
	SET_BIT(TIM3->EGR, TIM_EGR_CC2G);	//force interrupt
	__enable_irq();

 

 

 

Interrupt:

 

void TIM3_IRQHandler(){
	GPIOC->BSRR = (uint32_t) GPIO_PIN_3;
	if(READ_BIT(TIM3->SR, TIM_SR_CC4IF)){	// Torc PWM interrupt on CH4
		unsigned long captValue = TIM3->CCR4;	// read Capture register (resets interrupt flag)
		unsigned long lastRisingEdge = 0;
		unsigned long lastFallingEdge = 0;

		if(READ_BIT(GPIOB->IDR, GPIO_PIN_1)){	// Rising edge
			pwmDuty = (lastFallingEdge - lastRisingEdge) / (captValue - lastRisingEdge);
			lastRisingEdge = captValue;
		}
		else{	// Falling edge
			lastFallingEdge = captValue;
		}
	}

//	if(READ_BIT(TIM3->SR, TIM_SR_CC2IF)){	// Pedal rotation
//
//
//	}


	SET_BIT(TIM3->SR, 0xFFFFFFFF);//TIM_SR_CC2IF | TIM_SR_CC4IF); 	// Clear any int flags
	delayMicroseconds(1);
	GPIOC->BRR = (uint32_t) GPIO_PIN_3;
}

 

 

.I checked the pin, which is not floating nor receiving any relevant noise.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Still it is very strange, that after a resume of the debugger, the interrupt was not fired anymore. Furthermore it is even more strange, that i can not reproduce this issue after the next morning. I think there might be a little bug in the "de"-bugger. It also wont upload now anymore.