cancel
Showing results for 
Search instead for 
Did you mean: 

Timer for generating 1us tick

SShid
Associate III

I'm using STM32F108RG on 48MHz clock configuration.

I need to generate a 1 micrososeconds timer tick on it, for driving an output pin interfaced with a 3rd party device. Using PWM is not an option available.

I tried configuring TIM3 with following parameters:

Clock: Internal (48MHz)

Prescaler: 47 (48 - 1)

Counter Mode: Up

Counter Period (Auto-Reload Register -16 bit): 1

Internal Clock Division: No Division

Auto-reload preload: Disabled

With these settings, the closest I can reach is 6.8us.

I was able to generate 10us with the above settings with Counter Period set to 10,

but it doesn't seem to go below 6.8us.

I also tried TIM1 for the same purpose, but got the same observations.

Is that a limitation of the device, or do I need to perform any additional steps?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
SShid
Associate III

Thanks a lot for all your help, clive1.