cancel
Showing results for 
Search instead for 
Did you mean: 

Timer break function DMA request bit (BDE) documentation error (RM0091)?

zyss
Associate
Posted on May 11, 2016 at 12:27

In the description of a break function of TIM1 there is the following statement (in 16.3.12):

The break status flag (BIF bit in the TIMx_SR register) is set. An interrupt can be

 

generated if the BIE bit in the TIMx_DIER register is set. A DMA request can be sent if

 

the BDE bit in the TIMx_DIER register is set.

 

I really need this functionality, but there's no BDE bit neither in register description (16.4.4 - TIM1_DIER) nor in header files (CMSIS/stm32f030x6.h - no TIM_DIER_BDE bit).

Does this bit really exist in the STM32F0x MCU or it is a documentation error?

#stm32-rm0091-bde-dma-error
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on May 11, 2016 at 12:41

Same in RM0090 (for STM32F4xx) rev.11.

IMO that feature is missing, as there's no indication of timer-break DMA in the table of DMA sources.

It would be nice to hear a comment from ST.

JW