2018-12-15 2:32 AM
I am currently in a process of selecting micro controller for my project. Basically i need TTCAN support and i have STM32F746G Disco board with me. Now as per the ST reference manual i see that this is supported. Now my questions are...
ex: who will generate reference message(defined in TTCAN spec) ? HW or my SW?
3.Can i make STM32F746G as master of my TTCAN cluster ?
Unfortunately i could not find much details in the internet and the ST reference manual. If anybody has prior knowledge of working on this topic please do respond.
Thanks :| !!
Solved! Go to Solution.
2018-12-15 2:59 AM
Read the errata sheets. Since the first STM32 up to the STM32F76 there is an item:
"BxCAN time triggered mode not supported . "
2018-12-15 2:59 AM
Read the errata sheets. Since the first STM32 up to the STM32F76 there is an item:
"BxCAN time triggered mode not supported . "
2018-12-15 3:07 AM
Oh yes. I verified it. Thanks for saving my time and effort. BTW, is there any other MCU in ST which support TTCAN ?
2018-12-15 3:40 AM
STM32H7 and STM32L5.
tells that STM32G0x1 has FDCAM too, but rm0444 does not know about FDCAN.
2018-12-17 8:23 AM
Unfortunately, FDCAN does'nt serve the purpose !!.
do you know if ST has fixed this errata in subsequent HW releases? Ex: STM32F76. I cannot find any official Errata sheet for STM32F76x in ST websites.
2019-02-15 12:02 AM
CAN FD implemented in new STM32 MCU can be used as classic CAN, based on that you can use TTCAN.