2014-05-21 6:46 AM
Hi,
I use STM32F427 chip. In my application, I am generating a 25.6 kHz signal using an external signal with 9.984 MHz. In order to do so, the calculation for timer period should be as follows; (9.984MHz / 25.6kHz) - 1 = 389. However, in the application the microcontroller generates the 25.6 kHz when I set the timer period to 390. I am confused by that, shouldn't I subtract 1 by 390 to obtain the timer period? Thanks2014-05-21 7:11 AM
Yes, 390-1 should be the number, you'd want to consider how you are measuring the respective signals, and if the resynchronization of the input put might impact it.
2014-05-21 7:32 AM
I have a counter in my code to count the number of pulses that the timer generates. Also a PPS signal is connected to one of microcontroller pins which triggers an interrupt at each pulse. It turned out that when I check the number of pulses that counted between two PPS signals, it is exactly 25600 when period is 390, and it is 25666 when period is 389.
2014-05-21 7:33 AM
I have a counter in my code to count the number of pulses that the timer generates. Also a PPS signal is connected to one of microcontroller pins which triggers an interrupt at each pulse. It turned out that when I check the number of pulses that counted between two PPS signals, it is exactly 25600 when period is 390, and it is 25666 when period is 389.
2014-05-21 7:58 AM
Do you set directly the timer ARR register, or do you use some sort of ''library call'', which performs the decrement?
JW2014-05-22 3:45 AM
The piece of code that sets the timer period is below;
TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = 390; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);2014-05-22 7:23 AM
In reference manual it was written that the counter starts from 0 and counts to ARR value. I use PWM1 mode to generate the pulse, can this cause to counter to count from 1 to ARR value? It doesn't really make sense, but could this happen?
2014-05-22 7:49 AM
We would need to see all the relevant portions of your code to judge.
Can you measure the input and output frequency by some independent method, e.g. using a frequency counter? Or, alternatively, you can try two smaller ARR values to clearly see the difference - say, 10 and 11 - and have a look at the resulting waveform with an oscilloscope? JW2014-05-23 12:25 AM
I am posting the whole timer configuration code below;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; GPIO_InitTypeDef GPIO_InitStructure; TIM_ICInitTypeDef TIM_ICInitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB, GPIO_PinSource5, GPIO_AF_TIM3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_TIM3); TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = 390; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_ETRClockMode1Config(TIM3, TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted, 0); TIM_TIxExternalClockConfig(TIM3, TIM_TIxExternalCLK1Source_TI1, TIM_ICPolarity_Rising, 0); TIM_SelectSlaveMode(TIM3, TIM_SlaveMode_External1); TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); TIM_ICInitStructure.TIM_Channel = TIM_Channel_3; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICFilter = 0; TIM_SelectHallSensor(TIM3, ENABLE); TIM_ICInit(TIM3, &TIM_ICInitStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Disable; TIM_OCInitStructure.TIM_Pulse = 15; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset; TIM_OC2Init(TIM3, &TIM_OCInitStructure);