2018-03-25 9:02 AM
I have implemented on stm32f103xx the example TIM_ParallelSynchro, this not work. For stm32f407xx fine work.
int main(void)
{
HAL_Init();SystemClock_Config();InitConfigTIM3_Master();InitConfigTIM2_Slave();while (1)
{}
}static void InitConfigTIM2_Slave(void)
{ TIM_OC_InitTypeDef sOCConfig; TIM_SlaveConfigTypeDef sSlaveConfig; hTIM2.Instance = TIM2; hTIM2.Init.Period = 9; hTIM2.Init.Prescaler = 0; hTIM2.Init.ClockDivision = 0; hTIM2.Init.CounterMode = TIM_COUNTERMODE_UP; hTIM2.Init.RepetitionCounter = 0; HAL_TIM_Base_Init(&hTIM2);HAL_TIM_PWM_Init(&hTIM2);sOCConfig.OCMode = TIM_OCMODE_PWM1;
sOCConfig.OCPolarity = TIM_OCPOLARITY_HIGH; sOCConfig.Pulse = 3;HAL_TIM_PWM_ConfigChannel(&hTIM2, &sOCConfig, TIM_CHANNEL_3); sSlaveConfig.SlaveMode = TIM_SLAVEMODE_GATED; sSlaveConfig.InputTrigger = TIM_TS_ITR2; // for TIM3 masterHAL_TIM_SlaveConfigSynchronization(&hTIM2, &sSlaveConfig);HAL_TIM_MspPost_Init(&hTIM2);
HAL_TIM_PWM_Start_IT(&hTIM2, TIM_CHANNEL_3);
}static void InitConfigTIM3_Master(void)
{ TIM_MasterConfigTypeDef sMasterConfig; TIM_OC_InitTypeDef sOCConfig;hTIM3.Instance = TIM3;
hTIM3.Init.Period = 3600-1; hTIM3.Init.Prescaler = 0; hTIM3.Init.ClockDivision = 0; hTIM3.Init.CounterMode = TIM_COUNTERMODE_UP; hTIM3.Init.RepetitionCounter = 0; HAL_TIM_Base_Init(&hTIM3);HAL_TIM_PWM_Init(&hTIM3) ;sOCConfig.OCMode = TIM_OCMODE_PWM1;
sOCConfig.OCPolarity = TIM_OCPOLARITY_HIGH; sOCConfig.Pulse = 1800;HAL_TIM_PWM_ConfigChannel(&hTIM3, &sOCConfig, TIM_CHANNEL_2) ;sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;HAL_TIMEx_MasterConfigSynchronization(&hTIM3,&sMasterConfig) ;HAL_TIM_MspPost_Init(&hTIM3);
HAL_TIM_Base_Start_IT(&hTIM3);
HAL_TIM_PWM_Start_IT(&hTIM3, TIM_CHANNEL_2);}#tim_parallelsynchro-stm32f1032018-03-25 1:38 PM
Update event lasts only one cycle, which is not something very useful to use as a gate.
JW