2012-11-21 6:37 AM
I'm using the following code to update an output device, in this case the LCD, but when I enable TIM 2 the microcontroller stops working! what is wrong?
void Tim2_LCD_IT(void){
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
NVIC_InitTypeDef NVIC_InitStructure;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
//Configure TIM2
TIM_TimeBaseStructure.TIM_Period =((SystemCoreClock / 10000) / 2) - 1;
TIM_TimeBaseStructure.TIM_Prescaler = 10000 - 1;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);
TIM_Cmd(TIM2, ENABLE);
/* Enable TIM2 Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 3;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
void TIM2_IRQHandler(void){
TIM_ClearITPendingBit(TIM2,TIM_IT_Update);
LCD_command(Seconda_Riga); //Seconda riga
LCD_PrintData(Sprint,lenght(Sprint));
LCD_PrintData('' % '',13);
}
I also enabled another TIM to transmit data over the CAN, maybe there is some conflict?
void TIM4_IRQHandler(void)
{ //CAN TEST
TIM_ClearITPendingBit(TIM4,TIM_IT_Update);
TxMessage.Data[0] = 0x0F;
CAN_Transmit(CANx, &TxMessage);
}
void NVIC_Can_Config(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
NVIC_InitStructure.NVIC_IRQChannel = CAN2_RX0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 2;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
2012-11-21 7:42 AM
I'm using the following code to update an output device, in this case the LCD, but when I enable TIM 2 the microcontroller stops working! what is wrong?
Perhaps what you are trying to do under interrupt is inappropriate. ie Takes too long, has delays, or is dependent on other interrupt running.2012-11-21 8:34 AM
you are right, it is the management of the LCD that creates problems, thanks Clive, for all your great advice! :)