cancel
Showing results for 
Search instead for 
Did you mean: 

Threadx Link with static library

Venkat9010
Associate

Hello ST community,

           I am using STM32U585AIIQ6 micro controller I wanted a .c files to be as a static library i am using tx_thread_sleep one function of my .c files if those files are are included as a source file in my project the tx_thread_sleep is working out well but when I am using static library i am facing issue like no other thread is acquiring the CPU and moving into IDLE thread. I tried to change the priority but then also it doesn't worked out.Kindly please help me out as quick as possible I have delivery date in 2 days. 

Thank you 

Venkat sai

 

0 REPLIES 0