cancel
Showing results for 
Search instead for 
Did you mean: 

The STM32F407G-DISC1 board L1 ''fcm1608-0603'' inductor

Daniel Collado
Associate II
Posted on June 12, 2018 at 16:58

The STM32F407G-DISC1 board has an inductor L1 'fcm1608-0603' for power supplying purposes but the value does not appear, which is its value?

#inductor #power #stm32-disc1 #supply
4 REPLIES 4
AvaTar
Lead
Posted on June 13, 2018 at 09:01

Because it has a fixed value ?

https://www.tai-tech.com.tw/_upload/files/FCM1608-Series.pdf

 

Some while ago, I would perhaps have said 'Google Is Your Friend'. Not so sure anymore ...

Posted on June 13, 2018 at 09:46

 ,

 ,

But not even in the attached document is the inductance mentioned, I have

searched everywhere but I have not found it.

2018-06-13 9:03 GMT+02:00 AvaTar <,st-microelectronics@jiveon.com>,:

STMicroelectronics Community

<,https://community.st.com/?et=watches.email.thread>,

Re: The STM32F407G-DISC1 board L1 'fcm1608-0603' inductor

reply from AvaTar

<,

in STM32 MCUs Forum - View the full discussion

<,https://community.st.com/0D70X000006SqPhSAK

Posted on June 13, 2018 at 15:49

That component is not used as an inductor. It's a ferrite bead and meant to suppress certain frequencies. If you don't care about passing EMC tests you can use a short instead.

Posted on June 14, 2018 at 08:51

Ok, understood. By the way, in the document several are rated for different

DC resistance and MAX current. The one on the board will be a medium one

according to the current consumed by the uC?

2018-06-13 15:50 GMT+02:00 mich.lei <st-microelectronics@jiveon.com>:

STMicroelectronics Community

<https://community.st.com/?et=watches.email.thread>

Re: The STM32F407G-DISC1 board L1 'fcm1608-0603' inductor

reply from mich.lei

<

MCUs Forum* - View the full discussion

<https://community.st.com/0D70X000006Sy5GSAS