2013-10-17 3:53 AM
2013-10-17 7:34 AM
Don't know, but it looks like it's trying to generate an error, and jump to a user provided callback function to manage the error. I'd imagine that callback address is NULL, and thus not being called, and that R0 is some kind of ERROR CODE or context, which the callback could act upon.
The registers at the loop would likely be quite telling. At a guess it might be reporting it can't READ/WRITE the memory region passed, or it exceeds some limits?2013-10-17 7:48 AM
Passes through a string error message sent to
void GUI_Error(const char * s); void GUI_SetOnErrorFunc(void (* pFunc)(const char * s));http://www.segger.com/admin/uploads/productDocs/UM03001_emWin5.pdf
2013-10-23 12:15 AM
hello,cliver:
i found a problem.i used the st-link download the code and debug ,it can't pass the GUI_Init(),however ,i used the J-link ,it can .i don't know that's why . i have upgraded the firmware of the st-link.i don't know why?it's the dug of the st-link.or not? thanks.best regardsroyaizhixi@gmailc.om2015-04-24 4:47 AM
You will have to activate the CRC32 hardware peripheral. EmWin lib checks that way it is running on stm32 uC...
Tom2015-04-24 8:34 AM
2015-04-24 8:47 AM
You will have to activate the CRC32 hardware peripheral. EmWin lib checks that way it is running on stm32 uC...
Yeah thanks, 2013 called and already knew that, this is a DIFFERENT problem.
2015-04-27 1:38 AM
There is a bug with the Stlink code downloading. That's probably why it works for you using the Jlink, but does not if you use Stlink.
To verify this, just simply do a verification with the J-Flash, after you downloaded your code with Stlink, you'll most likely will get a comparison error.See my post: [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/St-link%20Error%20in%20HEX%20parser&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx?Paged%3DTRUE%26p_StickyPost%3D%26p_DiscussionLastUpdated%3D20150424%252000%253a44%253a12%26p_ID%3D52768%26View%3D%257bF47A9ED8%252dE726%252d42BE%252dACED%252d732F13B66581%257d%26FolderCTID%3D0x012001%26PageFirstRow%3D41¤tviews=22]Stlink hex error2015-04-27 5:47 AM
Ok, again this thread is from *2013* and Roy was *not* using ST-LINK Utilities, he'd been using IAR and KEIL directly. And had problems with memory buffers, and checks emWin did against them.
The errors with the ST-LINK Utilities .HEX parser, while interesting, don't impact most users where the debugger interfaces directly with ST-LINK. Everyone would be seeing problems, and that's simply not happening. The ST-LINK implementation is no where near as robust/industrial as the JLink, and it does a number of things differently which could explain issues short of gross ones where the memory is massively corrupted/shifted. Please can we stop digging up old threads with irrelevant input about unrelated problems you may have encountered in your own development efforts.