The question about RDP(STM32F401RE)
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-07-27 2:13 AM
Posted on July 27, 2016 at 11:13
Hi:
I used STM32F401RE nuclo board test RDP found that if i changed RDP level0 to level1 ,the code can't run. At the same time,i used the st-link utility to test it,found same question,i download the hex(LED demo) then update option bytes.At the end, reboot mcu by power up again,the code also can't run,i don't know why.i check the reference manual, can't found problem. Used st-linkutility
has problem,so i wanna use register to set the RDP level.follow is code:int main(void)
{ /* This sample code shows how to use STM32F4xx GPIO HAL API to toggle PA05 IOs connected to LED2 on STM32F4xx-Nucleo board in an infinite loop. To proceed, 3 steps are required: */ /* STM32F4xx HAL library initialization: - Configure the Flash prefetch, instruction and Data caches - Configure the Systick to generate an interrupt each 1 msec - Set NVIC Group Priority to 4 - Global MSP (MCU Support Package) initialization */ HAL_Init(); /* Configure the system clock to 84 MHz */ SystemClock_Config(); /* -1- Enable GPIOA Clock (to be able to program the configuration registers) */ __HAL_RCC_GPIOA_CLK_ENABLE(); /* -2- Configure PA05 IO in output push-pull mode to drive external LED */ GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FAST; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); HAL_FLASHEx_OBGetConfig(&myOp); if((myOp.RDPLevel&0xff)!=0xbb) { HAL_FLASH_Unlock(); HAL_FLASH_OB_Unlock(); myConfigOption();// // myOp.OptionType = OPTIONBYTE_RDP; // myOp.RDPLevel =tmp2;//0xff;// // HAL_FLASHEx_OBProgram(&myOp); // FLASH->OPTCR|=FLASH_OPTCR_OPTSTRT; HAL_FLASH_OB_Launch(); HAL_FLASH_OB_Lock(); HAL_FLASH_Lock(); } /* -3- Toggle PA05 IO in an infinite loop */ while (1) { HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5); /* Insert delay 100 ms */ HAL_Delay(100); }}void myConfigOption(){ FLASH_OB_RDP_LevelConfig(0xBB); //FLASH_OB_BOR_LevelConfig(OB_BOR_LEVEL2); }I can't find any problem, so i'm not sure where the problem is?Can you help me?Hardware ST Nuclo board STM32F401REIDE?IAR 7.4Firmware: STM32Cube1.9Tks BR Roy #stm32f401
Labels:
- Labels:
-
STM32F4 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-07-27 5:13 AM
Posted on July 27, 2016 at 14:13
I'd probably use a USART, or more GPIO outputs/modes, to try an gather how deep into the code it was getting, and report on the internal state as the device sees it .
My guess is that it is in a loop trying to get it into the option state you want. You aren't going to be able to use a debugger.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..