2024-09-01 11:14 PM
Hi Sir ,
I need your help with some questions about SPWMI:
1. STM32Cube_FW_H7_V1.7.0 without Demo project, Could you provide a Demo project of SWPMI STM32H7?
2. As RM said,SWPMI can serve only as Master interface, Whether SWPMI can communicate with itself ? such as Board1 SWPMI (transfer) communicate with Board2 SWPMI (receiver) .
3.When internal transceiver is bypassed(SWP_TBYP=1),the SWPMI_TX、SWPMI_RX and SWPMI_SUSPEND signals can connect an external transceiver. I don't find the profile about external transceiver.Could you please prodive the specific device or profile of external transceiver?
Looking forward to your reply!