2011-11-18 8:09 AM
My I2C routines are found with stm32F103C6 but when I ' ve make a migration to STM32L my I2C routines are not foun.
The I2C START BIT is not set when I call the I2C_GenerateSTART(I2C1, ENABLE); Anyone has been in the similar situation or issue? Please I need any help.. I attach my I2C configuration: ErrorStatus I2C_Start(void) { if (I2C_State == I2C_S_INITING) return ERROR; if (I2C_State == I2C_S_STOPPING) return ERROR; if (I2C_State != I2C_S_STOPPED) I2C_State = I2C_S_INITING; /* I2C1 Periph clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_Init(GPIOB, &GPIO_InitStructure); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); /* Enable APB1 I2C1 reset state */ RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C1, ENABLE); /* Release I2C1 from reset state */ RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C1, DISABLE); /* Enable the I2C EV Interrupt */ NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitStructure.NVIC_IRQChannel = I2C1_EV_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable the I2C ER Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = I2C1_ER_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* I2C1 Init */ I2C_InitTypeDef I2C_InitStructure; I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = 0x00; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = 100000; I2C_Init(I2C1, &I2C_InitStructure); I2C_Cmd(I2C1, ENABLE); I2C_State = I2C_S_WAITING; return SUCCESS; } Also before the startgenerate call I make: /* Interruption enabled */ I2C_ITConfig(I2C1, I2C_IT_EVT, ENABLE); I2C_ITConfig(I2C1,I2C_IT_BUF, ENABLE); I2C_ITConfig(I2C1,I2C_IT_ERR, ENABLE); Thanks in advance,2011-11-21 12:57 AM
The issue is resolved.
I must to remap the pins SDA and SCL to the ports. In the STM32F plattform is not necesssary. Bye everybody,