cancel
Showing results for 
Search instead for 
Did you mean: 

The HAL layer uses extra ram and generates more code

lo_529
Associate III
Posted on April 21, 2015 at 11:03

I am using CubeMx to generate my project code, it's really a good tools. But there's a new HAL layer in the generated code, which uses extra resources. I don't like this too much, so will there be an option that can disable the HAL code generate, using the ''StdPeriph_Lib'' only?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on April 21, 2015 at 16:28

In all honesty I don't see that ever happening. If you want to use the SPL then you'll need to own the code creation and integration task.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..