2009-04-20 11:06 PM
TFT LCD interfacing with the high-density STM32F10xxx FSMC
2011-05-17 04:09 AM
Hi,
I'm working with the STM3210E-EVAL board and RIDE7 with Rlink-PRO from RAISONANCE. I've downloaded the firmware of the ''AN2790: TFT LCD interfacing with the high-density STM32F10xxx FSMC'' and when I try to run the application it doesn't work. When the program is configuring the GPIOs, a ''HardFaultException'' appears and the program starts an infinite loop. I've just followed the written instructions in the readme.txt without any change :o Just in case, I have to say that I can run the examples of the FW library. Thanks.2011-05-17 04:09 AM
Hi,
The problem is solved. I've updated the RIDE7 and RKit-ARM to the last versions and the demo works without problems :-] Bye.