2024-09-07 10:02 PM
Hello,
I am configuring Nucleo-L073RZ with I-NUCLEO-LRWAN-1 expansion board in STM-Cube-IDE as the End-Node with the AT-Master Example in the en-cube-lrwan library provided by ST.
(en.i-cube_lrwan->STM32CubeExpansion_LRWAN_V2.1.0->Projects->NUCLEO-L073RZ->Applications->LoRaWAN->LoRaWAN_AT_Master->STM32CubeIDE->I_NUCLEO_LRWAN1)
Problem
When I Debug the code into the board it is halted at the HAL_INIT() function.
Solutions I tried
1. There are no breakpoints on it and just below it there a function call for clock configuration and I have also checked it.
2. Performed full chip erase after performing booting.
3. Checked on debugger configuration as well. (Reset Behaviour-> Connect under Reset)
I am attaching the log file also.
2024-09-07 11:10 PM
Hello @2001jolly
Could you add a screenshot of the projzct with all the files on the CubeIDE.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.