2011-01-19 8:51 AM
Systick priority
2011-05-17 5:21 AM
Why are you setting the SubPriority?
/* Configure the NVIC Preemption Priority Bits */
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);NVIC_SetPriority(SysTick_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
/* Enable the USART3 Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable the USART2 Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 2; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); You should also consider setting the priority AFTER using Systick_Config(), because it sets the LOWEST priority.2011-05-17 5:21 AM
Hi,
Thank you clive1 for your rapid answer !!!
I have spend 1 day to find this bug, without success.
I hav'nt seen that Systick_Config() set the lowest priority, and it is called after my priority setting.
Philippe