cancel
Showing results for 
Search instead for 
Did you mean: 

USB Host Library and USB PC Connection (HID Class)

kurtkraus2
Associate
Posted on January 19, 2011 at 22:00

USB Host Library and USB PC Connection (HID Class)

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andrew Neil
Super User
Posted on May 17, 2011 at 14:22

''As far i understood, there is no USB HID client and an USB Host available at the same time''

 

So, obviously, you will need two  USB ports - one as Host and the other as Client...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.