2019-05-29 5:31 AM
Hi,
I am currently working on an STM32L4S5 attached to a ST-LINK/V2. I am using Attolic TrueStudio to compile, flash and debug.
The STM32 is running at 120Mhz and I have configured the SWO clock to 125kHz thanks to the STlink utility software.
I am using the ITM_SendChar to sent data on port 0.
The issue is that I don't see any data on the SWV Console. I can observe and decode the data sended by the STM32 on the SWO port using an oscilloscope. I can confirm that I see the right data on the SWO port.
As far I can see, the issue should be between the STLink V2 and the Attolic TrueStudio sofware.
Have you ever experienced this issue or do you have ideas I could use to debug my issue ?
Thanks,
Regards,
Romain
2019-05-29 6:30 AM
Hi romain2,
Did you enable Serial Wire Viewer (SWD) in the debug configurations, with the correct core clock ?
Did you enable port 0 in the trace configurations ?
Did you click 'Start Trace' before launching your debug ?
Hope it could help a little bit.
Tristan
2019-05-29 7:03 AM
Hi tristan,
Thanks for your answer,
Yes everything you said as been set-up.
I have also tried another STLinkV2, no success.
Romain