2020-10-02 5:45 AM
Hi, I have 3 interruption pins PA13, PA14 and PA15, I would like to enable one pin for interruption at a time and changing the interruption mode, I made this function, but I'm not sure if it's the right way to achieve that.
void Switch(uint16_t PIN, uint32_t MODE)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
switch(PIN)
{
case GPIO_PIN_13:
GPIO_InitStruct.Pin = GPIO_PIN_14|GPIO_PIN_15;
GPIO_InitStruct.Mode = 0;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = PIN;
GPIO_InitStruct.Mode = MODE;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
break;
case GPIO_PIN_14:
GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_15;
GPIO_InitStruct.Mode = 0;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = PIN;
GPIO_InitStruct.Mode = MODE;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
break;
case GPIO_PIN_15:
GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_14;
GPIO_InitStruct.Mode = 0;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = PIN;
GPIO_InitStruct.Mode = MODE;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
break;
}
}I'm using a NUCLEO-L476.
2020-10-02 7:45 AM
Seems like it'll work if you call it with the right arguments. You should use "GPIO_InitStruct.Mode = GPIO_MODE_INPUT;" instead of 0 for clarity. You also need to enable the NVIC interrupt somewhere. Maybe you're doing that somewhere else.
2020-10-02 8:50 AM
It didn't work, choosing the pin any of the three pins didn't disable the interruption on other, I don't know if I'm doing something wrong but maybe I'm not calling correctly the interruption function:
Switch(GPIO_PIN_13, GPIO_MODE_IT_RISING);
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_8); // Diode
}