cancel
Showing results for 
Search instead for 
Did you mean: 

Switch from HSE to HSI on failure of the HSE?

sima2
Associate III
Posted on August 15, 2011 at 13:50

Hello

I would like to switch from the HSE oscilator to the HSI oscilator if there is a failure of the HSE oscilator. How can I do that with preserved SYSCLK (64MHz)?

The HSI klock is divided på 2 så the PLL would need to be changed by a factor of 2.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 15, 2011 at 14:32

PLLXTPRE (RCC_CFGR) permits you to feed HSE/2 into the PLL.

Although losing a synchronous clock, and switching a locked PLL to a different clock (even slightly), is a whole barrel of fun.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..