2015-12-30 3:37 PM
Hello,
I am currently developing a Visual C++ program that interacts with an STM32 via the STVP programming toolkit. Once this program is complete I plan to wrap it in an InstallShield installer. The documentation for the STVP programming toolkit specifies that STVP must be installed, is a redistributable version of this package available? At the very least is there some command line flag I can specify to put the regular installer in silent mode? I could just use the existing installer but it would be nice to reduce the amount of user interaction. Thanks, Alex #stvp #developer #redistributable2016-01-04 6:07 AM
Hi Alex,
There is no redistributable package for the toolset installer.You can add STVP files to your installer, after that install ST-Link drivers available under this you have to update your tool after each new version of toolset.-Shahrzad-