cancel
Showing results for 
Search instead for 
Did you mean: 

STVP Redistributable Package

athamm
Associate II
Posted on December 31, 2015 at 00:37

Hello,

I am currently developing a Visual C++ program that interacts with an STM32 via the STVP programming toolkit. Once this program is complete I plan to wrap it in an InstallShield installer. The documentation for the STVP programming toolkit specifies that STVP must be installed, is a redistributable version of this package available? At the very least is there some command line flag I can specify to put the regular installer in silent mode? I could just use the existing installer but it would be nice to reduce the amount of user interaction.

Thanks,

Alex

#stvp #developer #redistributable
1 REPLY 1
Posted on January 04, 2016 at 15:07

Hi Alex,

There is no redistributable package for the toolset installer.

You can add STVP files to your installer, after that install ST-Link drivers available under this

http://www.st.com/web/en/catalog/tools/PF260219

you have to update your tool after each new version of toolset.

-Shahrzad-