Strange behavior of IDE SW4STM32 in Code Editing and Debugging
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-12 12:18 AM - edited ‎2023-11-20 8:36 AM
I am using SW4STM32 (an Eclipse Variant) to code and debug my firmware, which is based on sample codes in package STM32Cube_FW_F4_V1.26.0.
I have observed two strange issue:
- IDE warns me that "Symbol '***' could not be resolved". However, it has no problem building the project.
- When I tried to do step-by-step debugging, the flow of steps is not as I expect them to be: it jumps. I do have a few callback functions, but the jumping does not happen between those callbacks; it happens in the initial stages of main.c before while loop, in which the callbacks are supposed to be called. During the init stage: a SPI with DMA, user button, LED, and USART with DMA are initiated and configured.
Anyone can shed some light?
- Labels:
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-12 8:27 AM
The IDE has a different idea of the project than the compiler, although the goal is for them to be the same.
Right click project -> Index -> Rebuild.
Cleaning the project and rebuilding may also help.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-13 12:04 AM
The editor migth no longer be cpmpatible....