2009-05-05 09:27 PM
STOne-32 - where is the pc tool for the boot loader
2011-05-17 04:11 AM
Hi STOne-32,
you wrote 2007 that you will soon have a tool for downloading firmware via the boot loader located the system memory of the STM32F10x. I want to use the USART1. Do you have the tool already? I can't find it - please help. I've tried several terminal programs but no one would be sufficient. By the way it is a great problem to send the 2 bytes for a command. It is easy to send 2 bytes direct one after the other. But that produces a NACK. If I send the 2 bytes with a timeout then I'll get a respond. But it is very difficult to send a ACK then. The way it works seems to be only useful with your tool, or not? Best regards pt1 [ This message was edited by: pt1 on 05-05-2009 18:58 ]2011-05-17 04:11 AM
Hi pt1,
Here you go :http://www.st.com/stonline/products/support/micro/files/um0462.zip
The link is located at this web link Cheers, STOne-32.2011-05-17 04:11 AM
Hi STOne-32,
you are my ''One'' and only :D . Thank you very much. Best regards pt1