cancel
Showing results for 
Search instead for 
Did you mean: 

STOne-32 - where is the pc tool for the boot loader

pt1
Associate II
Posted on May 06, 2009 at 06:27

STOne-32 - where is the pc tool for the boot loader

3 REPLIES 3
pt1
Associate II
Posted on May 17, 2011 at 13:11

Hi STOne-32,

you wrote 2007 that you will soon have a tool for downloading firmware via the boot loader located the system memory of the STM32F10x. I want to use the USART1. Do you have the tool already? I can't find it - please help.

I've tried several terminal programs but no one would be sufficient.

By the way it is a great problem to send the 2 bytes for a command. It is easy to send 2 bytes direct one after the other. But that produces a NACK. If I send the 2 bytes with a timeout then I'll get a respond. But it is very difficult to send a ACK then. The way it works seems to be only useful with your tool, or not?

Best regards pt1

[ This message was edited by: pt1 on 05-05-2009 18:58 ]

16-32micros
Associate III
pt1
Associate II
Posted on May 17, 2011 at 13:11

Hi STOne-32,

you are my ''One'' and only :-D . Thank you very much.

Best regards pt1