Skip to main content
lfor2007
Associate
August 14, 2015
Question

STMFlashLoader.exe version 2.7 doesn't recognize STM32F3_7x_8x_256K.STMAP

  • August 14, 2015
  • 5 replies
  • 1011 views
Posted on August 14, 2015 at 23:00

I'm trying to use ST's STMFlashLoader.exe program, which comes with the 

http://www.st.com/stonline/products/support/micro/files/um0462.zip

 package version 2.7. But in MSDoS, it is saying that: This version is not intended to support the <STM32F3_7x_8x_256K.STmap> target. 

Here are the steps I used:

1. 

STMFlashLoader.exe -c --pn 19 --br 4800 --to 7000 --pr EVEN --sb 1 --db 8

This step is OK.

2. STMFlashLoader.exe -i STM32F3_7x_8x_256K.STmap

This step has errors. 

Does anyone know the reasons?

Thanks in advance.

James

#stmflashloader.exe
    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    August 14, 2015
    Posted on August 15, 2015 at 01:06

    Did this STMAP file come in the 2.7 install? Or did you get it from somewhere else, or modify this?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    lfor2007
    lfor2007Author
    Associate
    August 16, 2015
    Posted on August 16, 2015 at 15:21

    Thank you. I do use the STmap provided by the version 2.7 without any modification.

    Amel NASRI
    ST Technical Moderator
    August 18, 2015
    Posted on August 18, 2015 at 12:20

    Hi lin.james.005,

    In UM0462, we have this description for STMFlashLoader.exe options:

    -i device_name

     

     

    Defines the MCU target to be used.For example: STM8_32K, STM32_Med-density_128K, STM32_High-density_512K,STM32_Low-density_16K etc. The device name is the name of the map file located in theMap directory

    So, you have to call:

    STMFlashLoader.exe -i STM32F3_7x_8x_256K

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Amel NASRI
    ST Technical Moderator
    August 18, 2015
    Posted on August 18, 2015 at 12:23

    Link to UM0462: http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00171488.pdf.

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    lfor2007
    lfor2007Author
    Associate
    August 18, 2015
    Posted on August 18, 2015 at 17:43

    You are right. The problem has been solved. Thank you very much. 

    Sincerely,

    James