cancel
Showing results for 
Search instead for 
Did you mean: 

STMF469I as I2S slave with external MEMS microphone

Posted on March 08, 2017 at 10:03

Hi.

I'm trying to understand the I2S configuration in STMF469I-Discovery. I've got external MEMS microphone that's outputting 16khz mono output. I can see with oscilloscope that the output is OK however I cannot seem to get the I2S configured correctly.

I've connected the mic like this and generated code with cubemx as I2S2 as slave with microphone outputting the clock signal (1Mhz), so no as SAI I2S input:

/**I2S2 GPIO Configuration

PB13 ------> I2S2_CK

PB12 ------> I2S2_WS

PC1 ------> I2S2_SD

I'm trying to read the output in task context like this:

 status = HAL_I2S_Receive(&hi2s2, buf, time * hi2s2.Init.AudioFreq, time*1000);

However the I2S_WaitFlagStateUntilTimeout expires as the while(__HAL_I2S_GET_FLAG(hi2s, Flag) == RESET) stays in RESET.

The HAL init is not the _weak definition stmf4xx_hal_i2s.c, but one _i2s_ex.c. Is this the problem or is this clock related?

I'm really having a hard time understanding the clock configuration and the audio pipelines as general. Is there any documentation about this? Below is the simple intialization generated by CubeMX and read function added by me.

/* I2S2 init function */

void MX_I2S2_Init(void)

{

hi2s2.Instance = SPI2;

hi2s2.Init.Mode = I2S_MODE_SLAVE_RX;

hi2s2.Init.Standard = I2S_STANDARD_LSB;

hi2s2.Init.DataFormat = I2S_DATAFORMAT_16B;

hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE;

//hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_44K;

hi2s2.Init.AudioFreq = I2S_FREQ;

hi2s2.Init.CPOL = I2S_CPOL_LOW;

hi2s2.Init.ClockSource = I2S_CLOCK_PLL;

hi2s2.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_DISABLE;

if (HAL_I2S_Init(&hi2s2) != HAL_OK)

{

Error_Handler();

}

}

void HAL_I2S_MspInit(I2S_HandleTypeDef* i2sHandle)

{

GPIO_InitTypeDef GPIO_InitStruct;

if(i2sHandle->Instance==SPI2)

{

/* USER CODE BEGIN SPI2_MspInit 0 */

/* USER CODE END SPI2_MspInit 0 */

/* Peripheral clock enable */

__HAL_RCC_SPI2_CLK_ENABLE();

/**I2S2 GPIO Configuration

PB13 ------> I2S2_CK

PB12 ------> I2S2_WS

PC1 ------> I2S2_SD

*/

GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_12;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

GPIO_InitStruct.Pin = GPIO_PIN_1;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;

HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

/* Peripheral DMA init*/

hdma_spi2_rx.Instance = DMA1_Stream3;

hdma_spi2_rx.Init.Channel = DMA_CHANNEL_0;

hdma_spi2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;

hdma_spi2_rx.Init.PeriphInc = DMA_PINC_DISABLE;

hdma_spi2_rx.Init.MemInc = DMA_MINC_ENABLE;

hdma_spi2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;

hdma_spi2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;

hdma_spi2_rx.Init.Mode = DMA_NORMAL;

hdma_spi2_rx.Init.Priority = DMA_PRIORITY_LOW;

hdma_spi2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

if (HAL_DMA_Init(&hdma_spi2_rx) != HAL_OK)

{

Error_Handler();

}

__HAL_LINKDMA(i2sHandle,hdmarx,hdma_spi2_rx);

/* USER CODE BEGIN SPI2_MspInit 1 */

/* USER CODE END SPI2_MspInit 1 */

}

}

void HAL_I2S_MspDeInit(I2S_HandleTypeDef* i2sHandle)

{

if(i2sHandle->Instance==SPI2)

{

/* USER CODE BEGIN SPI2_MspDeInit 0 */

/* USER CODE END SPI2_MspDeInit 0 */

/* Peripheral clock disable */

__HAL_RCC_SPI2_CLK_DISABLE();

/**I2S2 GPIO Configuration

PB13 ------> I2S2_CK

PB12 ------> I2S2_WS

PC1 ------> I2S2_SD

*/

HAL_GPIO_DeInit(GPIOB, GPIO_PIN_13|GPIO_PIN_12);

HAL_GPIO_DeInit(GPIOC, GPIO_PIN_1);

/* Peripheral DMA DeInit*/

HAL_DMA_DeInit(i2sHandle->hdmarx);

}

/* USER CODE BEGIN SPI2_MspDeInit 1 */

/* USER CODE END SPI2_MspDeInit 1 */

}

/* USER CODE BEGIN 1 */

HAL_StatusTypeDef get_i2s_data(uint16_t *buf, uint16_t time) {

   HAL_StatusTypeDef status;

   HAL_I2S_MspDeInit(&hi2s2);

   MX_I2S2_Init();

   status = HAL_I2S_Receive(&hi2s2, buf, time * hi2s2.Init.AudioFreq, time*1000);

   return status;

}

/* USER CODE END 1 */
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on March 08, 2017 at 12:09

Then its clock in RCC is probably off.

I don't Cube (as you might have guessed).

JW

View solution in original post

18 REPLIES 18
Imen.D
ST Employee
Posted on March 08, 2017 at 11:07

Hi,

I propose that you refer to the working I2S example within STM32CubeF4 firmware package. The provided example will help you to have more idea on how implementation is done:  

 STM32Cube_FW_F4_V1.15.0\Projects\STM324xG_EVAL\Examples\I2S\I2S_Audio

Refer to your reference manual in 'I2S functional description' section this may help you on your setting and more understanding the clock configuration.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
waclawek.jan
Super User
Posted on March 08, 2017 at 11:17

hi2s2.Init.Mode = I2S_MODE_SLAVE_RX;

So the mic is the source of clocks? Do you see both SCK and WS on PB13/PB12 with an oscilloscope/LA?

JW

waclawek.jan
Super User
Posted on March 08, 2017 at 11:44

And what is that flag Cube waits for? SPI_SR.RXNE? Do you observe the SPI/I2S registers in a debugger?

JW

Posted on March 08, 2017 at 11:48

I2S_FLAG_RXNE

From stm32f4xx_hal_i2s.c -> HAL_I2S_Receive

if (I2S_WaitFlagStateUntilTimeout(hi2s, I2S_FLAG_RXNE, RESET, Timeout) != HAL_OK)

{

return HAL_TIMEOUT;

}

My main confusion is the stm32f4xx_hal_i2sex -interface. Why the initialization is calling init there? What I understood from the code is that it's only for the full duplex stuff and not just for receiving.

Posted on March 08, 2017 at 12:06

All the SPI2 registers seem to be 0.

From debugger after timeout:

SPI2    SPI_TypeDef *    0x40003800    

    CR1    volatile uint32_t    0    

    CR2    volatile uint32_t    0    

    SR    volatile uint32_t    0    

    DR    volatile uint32_t    0    

    CRCPR    volatile uint32_t    0    

    RXCRCR    volatile uint32_t    0    

    TXCRCR    volatile uint32_t    0    

    I2SCFGR    volatile uint32_t    0    

    I2SPR    volatile uint32_t    0    
Posted on March 08, 2017 at 11:20

Thanks Imen!

The example is about playback. Is there anything about I2S slave input?

Also regarding the reference manual. Where do I get one that's applicable for 469i? I've found one that's for f43x.
Posted on March 08, 2017 at 11:24

Yes, there's valid activity on all lines. And the mic is outputting the as long as it's on.

Posted on March 08, 2017 at 12:27

If I understood correctly the cube clock tree, the I2S gets I2S_APB1_CLK (160Mhz). And RCC registers say that the APB1ENR has value 4143892991 (0xf6fec9ff). From stm32f469xx.h:

#define RCC_APB1RSTR_SPI2RST_Pos (14U)

#define RCC_APB1RSTR_SPI2RST_Msk (0x1U << RCC_APB1RSTR_SPI2RST_Pos) /*!< 0x00004000 */

#define RCC_APB1RSTR_SPI2RST RCC_APB1RSTR_SPI2RST_Msk

The bit is 1. Dunno about the rest of the clock config.

RCC    RCC_TypeDef *    0x40023800   

CR    volatile uint32_t    1057194115    

PLLCFGR    volatile uint32_t    624960527    

CFGR    volatile uint32_t    0    

CIR    volatile uint32_t    0    

AHB1RSTR    volatile uint32_t    0    

AHB2RSTR    volatile uint32_t    0    

AHB3RSTR    volatile uint32_t    0    

RESERVED0    uint32_t    0    

APB1RSTR    volatile uint32_t    0    

APB2RSTR    volatile uint32_t    0    

RESERVED1    uint32_t [2]    0x40023828    

AHB1ENR    volatile uint32_t    1050623    

AHB2ENR    volatile uint32_t    128    

AHB3ENR    volatile uint32_t    3    

RESERVED2    uint32_t    0    

APB1ENR    volatile uint32_t    270532608    

APB2ENR    volatile uint32_t    134234113    

RESERVED3    uint32_t [2]    0x40023848    

AHB1LPENR    volatile uint32_t    2129631231    

AHB2LPENR    volatile uint32_t    241    

AHB3LPENR    volatile uint32_t    3    

RESERVED4    uint32_t    0    

APB1LPENR    volatile uint32_t    4143892991    

APB2LPENR    volatile uint32_t    209157939    

RESERVED5    uint32_t [2]    0x40023868    

BDCR    volatile uint32_t    0    

CSR    volatile uint32_t    234881024    

RESERVED6    uint32_t [2]    0x40023878    

SSCGR    volatile uint32_t    0    

PLLI2SCFGR    volatile uint32_t    536883200    

PLLSAICFGR    volatile uint32_t    570432768    

DCKCFGR    volatile uint32_t    0    

EDIT: The clock config in main.c seems to be OK from what I understood from other examples.

Posted on March 08, 2017 at 11:57

Do you observe the SPI/I2S registers in a debugger?