2015-02-17 4:25 AM
When creating a project for the STM32103CBT6 where ADC1 is configured with 'Scan Conversion Mode' set to 'Enable' the code is generated incorrectly in MX_ADC1_INIT (adc.c).
The generated code shows: hadc1.Init.ScanConvMode = ENABLE;where ENABLE is defined as (!DISABLE) and DISABLE as 0
This should be: hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;where ADC_SCAN_ENABLE is defined as ADC_CR1_SCAN which is defined as ((uint32_t)0x00000100)
Also note that the ASSERT will be triggered with this generated code:assert_param(IS_ADC_SCAN_MODE(hadc->Init.ScanConvMode));STM32CubeMX v4.6.0 is used with STM32CubeF1 v1.0.02015-03-18 2:36 AM
Hello,
This is will be fixed with next 4.7 release.