cancel
Showing results for 
Search instead for 
Did you mean: 

STM32VLDiscovery - Input capture mode

hittive
Associate
Posted on November 25, 2014 at 13:08

Hi,

i want to capture time signal on PA0. I use a FreeRtos. My code:

//Input capture mode

    TIM1->CR1 = 0x0;

    TIM2->CCMR1=0x0;

    TIM2->CCER =0x0;

    TIM2->CR1 |=TIM_CR1_CMS ;

    TIM2->CR1 |=TIM_CR1_DIR;

    TIM2->CCMR1 |=TIM_CCMR1_CC1S_0 ;//  CC1 channel is configured as input, IC1 is mapped on TI1

    TIM2->CCMR1  |=TIM_CCMR1_IC1F_0 |TIM_CCMR1_IC1F_1 ;//f    SAMPLING N=8

    //TIM2->CCER |=TIM_CCER_CC1P ;//OC1 active high

    //TIM2->CCMR1&=~TIM_CCMR1_IC1PSC  ;//Prescaler

    TIM2->CCER|=TIM_CCER_CC1E; // Capture enabled

    //TIM2->CR1|=TIM_CR1_ARPE  ; autoreload

    TIM2->CR1|=TIM_CR1_CEN; // TIM2 enable

    TIM2->DIER|=TIM_DIER_CC1IE;// interrupt enable

    TIM2->PSC  = 23999;

    NVIC_EnableIRQ(TIM2_IRQn);

AND

   

void TIM2_IRQHandler(void)

{

    if(TIM2->SR &  TIM_SR_CC1IF)

    {

        TIM2->SR = ~TIM_SR_CC1IF;

    TIM2->CNT = 0;            //Zeruję licznik.

    ECHO=TIM2->CCR1;

    }

}

My signal on PA0 is PWM : 200ms high and 500ms low.

 ECHO=TIM2->CCR1 is alway 700. Why?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on November 25, 2014 at 14:49

>    TIM1->CR1 = 0x0;

TIM1? Probably a typo...

>    TIM2->CR1 |=TIM_CR1_CMS ;

Why???

> My signal on PA0 is PWM : 200ms high and 500ms low.

> ECHO=TIM2->CCR1 is alway 700. Why?

Because you capture on rising edge only. See CC1NP/CC1P in TIMx_CCER.

JW