2012-10-31 12:26 PM
Hi, i tried to use IAR example about LCD for use my display hd44780.
I connected 6 pin (RS,E,DB4,DB5,DB6,DB7) for use it on 4bit configuration (i'm sure that the connection is good cause i used that on my old arduino board). I only see first line of black simple, nothing else. Can someone help me with that code or link some other library that work good on stm32vldiscovery. Thx2012-11-11 10:24 AM
I just can link u this
, i see that some value is different from ur project, i hope it is helpful for u.2012-11-14 09:49 AM
I used the link before for rewrite my code, and it run good for 4bit configuration, if u haven't solved ur problem yet i can give u my code.
Bye2012-11-15 12:05 AM
I'm working on 8-bit, I have not adjusted the controls 4-bit, if you give me your code I check where is my error! thanks.
2012-11-15 12:56 AM