cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5G9J-DK2 MB1860A MB1860B differences and scheme for A version

wegi01
Associate III

I got STM32U5G9J-DK2 and this Discovery is still assembled with LCD board MB1860A version.

MB1860A - STM32U5G9J-DK2.jpg

But the documentation suggesting this DK have LCD board MB1860B version and share only B version scheme.

CUBE_SCH_PACK.png

I taked damage of my LCD board MB1860A and replaced it to MB1860B LCD board version from my next Discovery Kit STM32H7S78-DK.

MB1860B.jpg

And here arising some problems:

For example the BSP demo from example pack working flawlesly, but the main demo embedded from factory doesn't work with STM32U5G9J-DK2  and MB1860B version of LCD board. The LCD is dark and look as dead.

 

So my questions  which could be provide the answer about incorrectly work of LCD sounds like:

1. Why doesn't the main demo work, despite of the docimentation suggestion that this kit is assembled with the MB1860B LCD version board?

2. How I can obtain the scheme for MB1860A LCD board version?

3. What are the differences between the MB1860A and MB1860B board versions?

4. What should I do to make the main demo work with STM32U5G9J-DK2 and the MB1860B LCD board version?

 

Thank you kind in advance for any information.

 

0 REPLIES 0