cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U575xx USB

joaorego
Associate

Hello,

Does the STM32U575CG/I (48-pin package) support USB communication, or is USB functionality only available on higher pin-count variants?

Thank you.

4 REPLIES 4
FBL
ST Employee

Hi @joaorego 

All packages for this family support USB!

FBL_1-1739955901488.png

575 = STM32U575xx with OTG

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

But what about the USB supply voltage? Will it be sourced directly from VDD? Can I still supply VDD with a voltage lower than 3V?

joaorego_0-1739956528083.png

 

gbm
Principal

USB requires  3.3 V power.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
FBL
ST Employee

Hi @joaorego 

As explained in the footnote of Table 150. OTG_FS characteristics (continued) in page 304,

USB functionality is ensured down to 2.7V, but some USB electrical characteristics are degraded in 2.7 to 3.0 V range.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL