cancel
Showing results for 
Search instead for 
Did you mean: 

stm32u575 & Ethernet port

mauroalba
Associate II

Hi,

I've a board, now a nucleo-u575zi-q but i'm waiting for a custum boad based on same MCU. I need this serie for the low power functionalities. In next phase of project , in this board i need an ethernet port where run web and tcp server. I found some good examples about these features but are all based on different series of MCU. There are examples based on STM32F and H series, both have a specific set of pins to manage the ethernet connection defined as ETH block.  They use Azure or Freertos with or without Lwip in conjunction with Lan8742 component as physical interface. My question is: can i use the same eth components, hw and sw, also with STM32U5 series? The functionalities used in eth micro block can be replicated, are only gpio pins to configure?, in U series ? In this way i can start from examples already present or i need to change MCU to have eth port on board? 

Thanks

5 REPLIES 5
mƎALLEm
ST Employee

Hello,

You can use LAN8742 with STM32U5 MCU but you don't have it on the NUCLEO-U575ZI-Q board.

Do you plan to add an external ETH PHY module? 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mauroalba
Associate II

Yes, i'll add externally the LAN8742 component/board. My dubts are about the configuration of "specific" block inside MCU.

Unfortunately there is no ready to use ETH example on U5. You need to inspire from other products ETH examples.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mauroalba
Associate II

yes, i saw this. My goal would be use in U575 netxduo using th examples developed for F/H series with Lan8742 so to not have to write driver. If im not wrong netxduo natively support this eth interface.