2024-06-12 3:45 AM - edited 2024-06-12 4:18 AM
Hi community people,
As an introduction, please note I'm completely new to the STM32 world, and back in embedded world after a long break in the application level. I now jump in a new project that will be based on a STM32U5, and I start digging in documentation, code examples and ST ecosystem (MX, IDE etc.).
I tried to find answer to my question, but failed. Either I did not look correctly, and I apologise in that case, or the answer does not exist.
Here it is : the Nucleo-U575IZ-Q comes loaded with a demo software : LEDs (led1, led2, led3) blink change, and the speed changes according to the number of press on the user button. Appnote UM2861 says the source code can be downloaded from ST.com but I failed to find it. I have MCU package installed, and I do not find it in the source tree also.
If you can point me to the source code of that exemple (and a IAR project is a cherry on the cake), I'll be very happy
Thanks in advance
Patrice
2024-06-12 4:24 AM
They used to have a Demo directory, Not seeing on the current GitHub, but this might be a close substitute
2024-06-12 5:01 AM
Hi,
This make sense, I will give it a try. Thank you
2024-06-12 7:14 AM
Hi @Tesla DeLorean on both github and locally on my laptop (I downloaded and installed the latest MCU package that I assume is somehow cloning the GH repo), this sample is not matching the pre installed demo app in the Nucleo board.
Not a big deal anyway, there is plenty of examples to look at, but the one on the board.
2024-06-12 10:03 AM
Hi @PatriceL
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2024-06-13 12:22 AM
Hi @Billy OWEN I did not expect my first post here was going to escalate this quick ;) . Thank you anyway to consider this.