cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4xx: standby and run mode

Paolo Andreuzza
Associate II
Posted on November 03, 2017 at 14:07

Hallo,

Since I think that the use of auto generated code using MXcube helps a lot, I have a question regarding the best workflow to use in the following case.

My board is powered by an external power source. In this state it works at full speed. When the external power source is disconnected, the MCU goes in standby to reduce the power consumtion because, in this state, it is powered by a coin cell. The only thing it has to do is wakeup (using the RTC) every 100 mS to check some gpio and then it has to go again in standby.

there is a gpio that inform the MCU if it is powered by the button battery or by the external supply.

In this case it seems to me that I need of two different MCU setup depending on wich power source is feeding the board.

It is not an easy situation for MXCube, is it?

Ideas?

Thank you in advance.

Paolo
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on November 03, 2017 at 14:57

Hello!

In main function , just before call  HAL_Init(), write some code  (not using HAL) that enables GPIO pin and check the state. If met the proper condition, continue to initialize HAL or  LL  , else put it again to STBY. 

A minimal piece of code with no extra clock configurations and no necessary peripherals initialization, helps to maintain  the battery's life.

CubeMx produces a 'standard' type of initialization code and can't do this.

regards

vf

View solution in original post

2 REPLIES 2
Posted on November 03, 2017 at 14:57

Hello!

In main function , just before call  HAL_Init(), write some code  (not using HAL) that enables GPIO pin and check the state. If met the proper condition, continue to initialize HAL or  LL  , else put it again to STBY. 

A minimal piece of code with no extra clock configurations and no necessary peripherals initialization, helps to maintain  the battery's life.

CubeMx produces a 'standard' type of initialization code and can't do this.

regards

vf

Posted on November 03, 2017 at 15:24

It was even my thought, but i were not so sure...

thank you very much