2016-07-13 5:31 AM
Hello,
the HAL function HAL_CAN_Transmit_IT() enables the Transmit mailbox empty Interrupt before the requesting transmission. At least if I run the CAN bus wit 1Mbit the mailbox empty interrupt is triggered before the new frame is send. I read abaut this problem in this forum before but also new HAL drivers are delivered with the same bug! #can-interrupt-transmission2016-07-13 6:53 AM
Hi,
It is a known bug which is confirmed by ST team, but the fix has not yet been released.Regards2016-07-14 8:23 AM
Hi,
Please explain with more details your problem, maybe is not the same issue that I have a look in this forum.It's possible to share discussions which contains this problem?Regards