STM32L496G-Discovery PSRAM problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-11-08 1:04 AM
Posted on November 08, 2017 at 10:04
Hey, I'm using STM32L496G-Discovery before our PCBA will arrive. According to the docs there is 8Mbit
(1MB) PSRAM on board, but in ALL ST examples with the board just 64k of it defined into icf (from 0x1000000 to 0x1000ffff), I use IAR IDE. When I try to change it to 1MB (from 0x1000000 to 0x100fffff) I receive HW fault at debugger power up state). LCD shares bus with PSRAM, I disconnected it, but still it doesn't help. Could someone help and provide the way for (if needed) hw modifications and configuration in order to use whole 1MB PSRAM space.Thanks,
Boris
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-11-08 3:37 PM
Posted on November 09, 2017 at 00:37
When I try to change it to 1MB (from 0x1000000 to 0x100fffff) I receive HW fault at debugger power up state).
Where do you change that, and what are the material consequences of that change?
JW