cancel
Showing results for 
Search instead for 
Did you mean: 

stm32l476 External interrupt

Boris Fi
Associate
Posted on March 07, 2018 at 09:15

Hi,

I am trying to use external interrupt. 

I connect the PB3 to external output and I want to detect ricing voltage.

I Using microcontroller STM32L476RG on Nucleo-L476RG.

Moreover,

I found the example that explained how use external interrupts on

https://community.st.com/external-link.jspa?url=https%3A%2F%2Fwww.youtube.com%2Fwatch%3Fv%3DuKwD3JuRWeA

. In my code I changed to PB3.

But Something wrong.

This is my small code.

May anyone can detect the problem?

I using Microcfor ARM Compiler.

static int SlowSpeedFlag = 0;

void external_interrupt() iv IVT_INT_EXTI3 ics ICS_AUTO

{

      if((EXTI_PR1 & PR3) != 0)   //Check if PE11 has trigger the interrupt

      {

          EXTI_PR1 |= PR3;

          SlowSpeedFlag = 1;

      }

}

//-----------------------------------------------------------------------------------//

void main()

{

     GPIO_Digital_Output(&GPIOA_BASE, _GPIO_PINMASK_5);  //Led2 on Nucleo Board

     GPIOA_ODR = 0;

     GPIO_Digital_Input(&GPIOC_IDR, _GPIO_PINMASK_13);   //Button On Nucleo Board

     GPIOC_ODR = 0;

     EnableInterrupts();                //Enable global interrupt

     //RCC_AHB2ENR.B1 = 1;

     GPIOBEN_bit = 1;

    

     GPIO_Config(&GPIOB_BASE,_GPIO_PINMASK_3, _GPIO_CFG_MODE_INPUT | _GPIO_CFG_PULL_DOWN);

     NVIC_IntEnable(IVT_INT_EXTI3);      //Enable NVIC interface

    

     //RCC_AHB2ENR.B0 = 1;

     SYSCFGEN_bit = 1;

     //SYSCFG_EXTICR1.B2 = 1;

     EXTI02_bit = 1;

     //SYSCFG_EXTICR1.B1 = 0;

     EXTI01_bit = 0;

     //SYSCFG_EXTICR1.B0 = 0;

     EXTI00_bit = 0;

     EXTI_RTSR1.TR3 =  1;            //Rising trigger enabled (for Event and Interrupt) for input line

     EXTI_IMR1.MR3 = 1;              //Interrupt request from Line x is not masked

     EXTI_EMR1.B3 = 1;               //Event request from line x is not masked

     while(1)

     {

        if(SlowSpeedFlag == 0)

            Delay_ms(500);

        else

            Delay_ms(100);

        

        

        //if button pressed, the speed of led blinking will changed

        if(IDR13_GPIOC_IDR_bit == 0)

        {

           if(SlowSpeedFlag == 0)

              SlowSpeedFlag = 1;

           else if(SlowSpeedFlag == 1)

              SlowSpeedFlag = 0;

             

           while(IDR13_GPIOC_IDR_bit==0);

        }

        GPIOA_ODR.B5 = !GPIOA_ODR.B5;  //Togle Led2 on Nucleo Board

    }

}

#interrput
2 REPLIES 2
Posted on March 07, 2018 at 11:41

Read out in debugger, and check/post the relevant GPIO/SYSCFG/EXTI registers.

Try if you've set correctly the interrupt, by triggering the EXTI by writing to respective bit of EXTI_SWIER1.

JW

Andrew Neil
Evangelist III
Posted on March 07, 2018 at 12:38

I using Microcfor ARM Compiler.

You mean

MicroC for ARM -

  

this: 

https://www.mikroe.com/mikroc-arm

  ?

What does all this mean:

void external_interrupt() iv IVT_INT_EXTI3 ics ICS_AUTO

Are you sure that's correct?