2018-07-10 2:14 AM
Hello, Help me please. I configuration STM32L452RET6 in the CUBEMX, how on the pictures. Then I build project in the Attolic and go to debuger and then when MCU is starting work, it go in the HardFault_Handler(void) through 1-5 seconds. Why? I can't find problem. Maybe anyone know?
Crystal clock is Abracon LLC ABM9- 8.000MHZ-10-D-1U-T.
/** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** *//* Includes ------------------------------------------------------------------*/&sharpinclude 'main.h'&sharpinclude 'stm32l4xx_hal.h'/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*//* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);static void MX_GPIO_Init(void);/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*//* USER CODE END PFP */
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point. * * @retval None */int main(void){ /* USER CODE BEGIN 1 *//* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init(); /* USER CODE BEGIN 2 *//* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */ while (1) { HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_12); HAL_Delay(300); /* USER CODE END WHILE *//* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */}
/**
* @brief System Clock Configuration * @retval None */void SystemClock_Config(void){RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); }/**Enables the Clock Security System
*/ HAL_RCC_EnableCSS();/**Configure the main internal regulator output voltage
*/ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure the Systick interrupt time
*/ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}/** Configure pins as
* Analog * Input * Output * EVENT_OUT * EXTI*/static void MX_GPIO_Init(void){GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE();/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_12, GPIO_PIN_RESET);/*Configure GPIO pin : PA12 */
GPIO_InitStruct.Pin = GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief Period elapsed callback in non blocking mode * @note This function is called when TIM2 interrupt took place, inside * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment * a global variable 'uwTick' used as application time base. * @param htim : TIM handle * @retval None */void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){ /* USER CODE BEGIN Callback 0 *//* USER CODE END Callback 0 */
if (htim->Instance == TIM2) { HAL_IncTick(); } /* USER CODE BEGIN Callback 1 *//* USER CODE END Callback 1 */
}/**
* @brief This function is executed in case of error occurrence. * @param file: The file name as string. * @param line: The line in file as a number. * @retval None */void _Error_Handler(char *file, int line){ /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ while(1) { } /* USER CODE END Error_Handler_Debug */}&sharpifdef USE_FULL_ASSERT
/** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, tex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */ /* USER CODE END 6 */}&sharpendif /* USE_FULL_ASSERT *//**
* @} *//**
* @} *//************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
#stm32l452 #stm32l4 #no-working-hse-stm32l42018-07-11 4:03 AM
I am cheking clock signal on the MCO pin and signal is very good.
I checkdefine for HSE_VALUE in stm32xxxx_hal_conf.h. It is 8 MHz.
If I stand crystal clock on the 16 MHz and AHB Prescaler = 2, board is working. But if I stand crystal clock on the 8 MHz, MCU go to
HardFault_Handler(void) on the Debagger mode. But if I disconnect Debugger, and reseting MCU. MCU work stably. Why? Do you know?
2018-07-11 5:13 AM
Read out the content of relevant RCC registers in case of problem and check/post.
JW
2018-07-11 5:21 AM
Hi Anton,
In both configuration case, are you able to debug step by step your SystemClock_Config() function by placing a breakpoint at the beginning. Then step into HAL_RCC_OscConfig(&RCC_OscInitStruct) to troubleshoot the Hard Fault ?
In addition, what is your hardware? Is it a board that you designed yourself? Or a NucleoL452?
BR
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.