cancel
Showing results for 
Search instead for 
Did you mean: 

STM32l433 + M25P16 + FatFs ... File system not working

deepak23
Associate
Posted on October 03, 2016 at 11:09

Hi all ,

I am currently with stm32l433, where i am stuck between FatFs file system. There are few things i need to clear.

1. Communication between STM32L433 and M25p16 working properly with help of SPI. All read and write operation working .

The Problem is : 

When i am trying to put Fatfs which was generated by CubemX , then i am getting error that ''No File System Found''.

So my first Question :

1. Is M25P16 Flash supports FatFs (

elm-chan.org/fsw/ff/00index_e.html

)  ?

2. If it is supported what will be the steps i need to follow to overcome this problem.

3. If it is not supported then, what other File system can i use with my external m25p16 memory device ?

 

2 REPLIES 2
Walid FTITI_O
Senior II
Posted on October 04, 2016 at 18:15

Hi singh.deepak.002, 

You may check in open project source communities like Github : for example this

https://github.com/gk969/stm32-speech-recognition/blob/master/BSP/M25P16.c

( no confirmation of the code's wellness )

-Hannibal-

Posted on October 04, 2016 at 18:41

Unless the flash has been formatted/initialized it is not going to have FAT MBR or BPB data or structures on it. ie No File System

1) Don't know, can you read/write 512 byte sector(s) properly?

2)

http://elm-chan.org/fsw/ff/en/mkfs.html

() the media? See also

http://elm-chan.org/fsw/ff/en/fdisk.html

()

http://elm-chan.org/fsw/ff/en/appnote.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..